There are no products listed under this brand.
Call: 1.800.289.2779
HELI-COIL / STANLEY ENGINEERED FASTENING
HeliCoil, a STANLEY Engineered Fastening brand, is known around the world as the original wire insert that is installed into soft metallic materials creating a maximum strength performance. These inserts have allowed the light-weight manufacturing sector to use materials such as aluminum without sacrificing thread strength. Heli-Coil inserts are available both tanged and tangless.
Hand and power installation tools, gages and tang break-off tools are also available.
There are no products listed under this brand.